cancel
Showing results for 
Search instead for 
Did you mean: 

motor_control_with_evspin

dineshsharma2025
Associate II

Hi i am getting this error while opening motor pilot for gui in motor control,pls go throgh below attached file.

 

 
 

 

2 REPLIES 2
DigitalMonk123
Associate

This error usually means the COM port is open but the board isn’t responding—ensure the correct COM port and baud rate are selected, and that the firmware on your STM32 is running with Motor Control UART enabled. Also check cable, drivers, and that no other software is using the same port.

GMA
ST Employee

Hello @dineshsharma2025,

Check also Baudrate speed (set to 115200 on your snapshot).
image.png

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA