2018-06-08 1:52 PM
Hi all,
I'm trying to get started with the Motor Control SDK 5.1.0, after viewing the webinar. Hardware is a Nucleo F302R8, Nucleo-IHM07M1 (in 3 shunt configuration), and the bullrunning 1700 kV motor. The motor profiler runs, although I couldn't get it working (it doesn't give stable rotation). That's ok for now, as it indicates the HW/SW platform is in working condition.
The steps taken are as follows:
- Use MCSDK 5.1.0 with the hardware mentioned above, to generate an .ioc file. For code generation, SW4STM32 is selected.
- Open the .ioc file in STM32CubeMX 4.26.0
- Generate code, and click 'open project', which opens SW4STM32
- Build the project in SW4STM32. The building runs quite far, until the following error is thrown:
Building target: motorTestC.elf
Invoking: MCU GCC Linkerarm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -specs=nosys.specs -specs=nano.specs -T'../STM32F302R8Tx_FLASH.ld' -Wl,-Map=output.map -Wl,--gc-sections -o 'motorTestC.elf' @'objects.list' -lmApplication/User/mc_tasks.o: In function `MCboot':C:/PATH/motorTestC/Src/mc_tasks.c:184: undefined reference to `STO_PLL_Init'C:/PATH/motorTestC/Src/mc_tasks.c:188: undefined reference to `RUC_Init'Application/User/mc_tasks.o: In function `TSK_MediumFrequencyTaskM1':C:/PATH/motorTestC/Src/mc_tasks.c:308: undefined reference to `STO_PLL_CalcAvrgMecSpeed01Hz'C:/PATH/motorTestC/Src/mc_tasks.c:337: undefined reference to `RUC_Clear'C:/PATH/motorTestC/Src/mc_tasks.c:339: undefined reference to `STO_PLL_Clear'C:/PATH/motorTestC/Src/mc_tasks.c:353: undefined reference to `RUC_Exec'C:/PATH/motorTestC/Src/mc_tasks.c:367: undefined reference to `STO_PLL_IsObserverConverged'Application/User/mc_tasks.o: In function `TSK_HighFrequencyTask':C:/PATH/motorTestC/Src/mc_tasks.c:647: undefined reference to `RUC_FirstAccelerationStageReached'C:/PATH/motorTestC/Src/mc_tasks.c:650: undefined reference to `STO_PLL_CalcElAngle'C:/PATH/motorTestC/Src/mc_tasks.c:651: undefined reference to `STO_PLL_CalcAvrgElSpeedDpp'C:/PATH/motorTestC/Src/mc_tasks.c:654: undefined reference to `STO_ResetPLL'Application/User/user_interface.o: In function `UI_SetReg':C:/PATH/motorTestC/Src/user_interface.c:270: undefined reference to `STO_PLL_GetObserverGains'C:/PATH/motorTestC/Src/user_interface.c:271: undefined reference to `STO_PLL_SetObserverGains'C:/PATH/motorTestC/Src/user_interface.c:290: undefined reference to `STO_PLL_GetObserverGains'C:/PATH/motorTestC/Src/user_interface.c:291: undefined reference to `STO_PLL_SetObserverGains'C:/PATH/motorTestC/Src/user_interface.c:310: undefined reference to `STO_GetPLLGains'C:/PATH/motorTestC/Src/user_interface.c:311: undefined reference to `STO_SetPLLGains'C:/PATH/motorTestC/Src/user_interface.c:331: undefined reference to `STO_GetPLLGains'C:/PATH/motorTestC/Src/user_interface.c:332: undefined reference to `STO_SetPLLGains'Application/User/user_interface.o: In function `UI_GetReg':C:/PATH/motorTestC/Src/user_interface.c:591: undefined reference to `RUC_GetNumberOfPhases'C:/PATH/motorTestC/Src/user_interface.c:520: undefined reference to `STO_GetPLLGains'C:/PATH/motorTestC/Src/user_interface.c:500: undefined reference to `STO_PLL_GetObserverGains'C:/PATH/motorTestC/Src/user_interface.c:480: undefined reference to `STO_PLL_GetObserverGains'C:/PATH/motorTestC/Src/user_interface.c:540: undefined reference to `STO_GetPLLGains'C:/PATH/motorTestC/Src/user_interface.c:694: undefined reference to `STO_PLL_GetEstimatedCurrent'C:/PATH/motorTestC/Src/user_interface.c:800: undefined reference to `STO_PLL_GetEstimatedBemfLevel'C:/PATH/motorTestC/Src/user_interface.c:818: undefined reference to `STO_PLL_GetObservedBemfLevel'C:/PATH/motorTestC/Src/user_interface.c:748: undefined reference to `STO_PLL_GetEstimatedBemf'C:/PATH/motorTestC/Src/user_interface.c:730: undefined reference to `STO_PLL_GetEstimatedBemf'C:/PATH/motorTestC/Src/user_interface.c:712: undefined reference to `STO_PLL_GetEstimatedCurrent'Application/User/user_interface.o: In function `UI_GetRevupData':C:/PATH/motorTestC/Src/user_interface.c:1005: undefined reference to `RUC_GetPhaseDurationms'C:/PATH/motorTestC/Src/user_interface.c:1006: undefined reference to `RUC_GetPhaseFinalMecSpeed01Hz'C:/PATH/motorTestC/Src/user_interface.c:1007: undefined reference to `RUC_GetPhaseFinalTorque'Application/User/user_interface.o: In function `UI_SetRevupData':C:/PATH/motorTestC/Src/user_interface.c:1032: undefined reference to `RUC_SetPhaseDurationms'C:/PATH/motorTestC/Src/user_interface.c:1033: undefined reference to `RUC_SetPhaseFinalMecSpeed01Hz'C:/PATH/motorTestC/Src/user_interface.c:1034: undefined reference to `RUC_SetPhaseFinalTorque'Application/User/mc_config.o:(.data+0x2d4): undefined reference to `STO_PLL_ForceConvergency1'Application/User/mc_config.o:(.data+0x2d8): undefined reference to `STO_PLL_ForceConvergency2'Application/User/mc_config.o:(.data+0x2dc): undefined reference to `STO_OTF_ResetPLL'Application/User/mc_config.o:(.data+0x2e0): undefined reference to `STO_PLL_IsVarianceTight'collect2.exe: error: ld returned 1 exit statusmakefile:37: recipe for target 'motorTestC.elf' failedmake: *** [motorTestC.elf] Error 1Can anyone explain why this happens, and how it can be solved? Thanks a lot in advance! In case additional input is needed, feel free to ask.
Solved! Go to Solution.
2018-06-09 4:24 PM
Hi
klopwouter
,From the error message, it prompts that the lib of mc was missing from link.
To manually fix the problem, you can go 'project properties' --> 'C/C++ Build' --> 'Settings' --> 'Tools settings' --> 'MCU GCC Linker' --> 'Libraries'
in 'Libraries (-l)' , add :libmc-truestudio_M4.lib
in 'Library searching path (-L)' , add ../../../MCSDK_v5.1.0/MotorControl/lib
Hope this will help.
BTW, the sw4stm32 and truestudio both use GCC, so the lib was shared.
-Andy
2018-06-09 4:24 PM
Hi
klopwouter
,From the error message, it prompts that the lib of mc was missing from link.
To manually fix the problem, you can go 'project properties' --> 'C/C++ Build' --> 'Settings' --> 'Tools settings' --> 'MCU GCC Linker' --> 'Libraries'
in 'Libraries (-l)' , add :libmc-truestudio_M4.lib
in 'Library searching path (-L)' , add ../../../MCSDK_v5.1.0/MotorControl/lib
Hope this will help.
BTW, the sw4stm32 and truestudio both use GCC, so the lib was shared.
-Andy
2018-06-10 4:13 AM
Hi
Blue.Andy
,Thanks for the quick reply! Your solution works perfect. One small addition is that the lib folder was not available in the project folder, so I copied the lib folder from the Program files directory.
Thanks a lot for helping me out
2021-06-15 1:26 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards