cancel
Showing results for 
Search instead for 
Did you mean: 

spin3201 dont work with st-motor-control 5.2

Posted on May 30, 2018 at 08:47

Hello, I downloaded the latest version of st-motor-control. When I open an example, the software informs me that I am using a newer version and must migrate from 4.3 to 5.0.2. I accept.

Now, 

I can open the monitor window and I can control the engine. If I want to modify the configuration and generate it, the software informs me that I can not do it because 'F1 mcus not supported in FW for SDK 5.0'

When I load the example, I have the following information:

App: STMCWB

Time: 05/30/2018 08:38:42

Project: Noname

Filename: F:\MHK\STM32\STEVAL3201\Noname.log

Type Time Motor Id Message

UNK 08:06:41 The 'Sensor-less (HFI+Observer)' is not supported in the FW for SDK5.0. All parameters will be disabled.

UNK 08:06:41 The 'PFC' is not supported in the FW for SDK5.0. All parameters will be disabled.

UNK 08:06:41 The 'LCD' is not supported in the FW for SDK5.0. All parameters will be disabled.

UNK 08:06:41 F1 mcus are not supported in the FW for SDK5.0

UNK 08:06:41 F2 mcus are not supported in the FW for SDK5.0

UNK 08:06:41 STSPIN mcu is not supported in the FW for SDK5.0

Where can I find an sDK vesion 4.3 ?

Thank.

Christian

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
cedric h1
Associate III
Posted on June 11, 2018 at 12:57

Dear Christian,

STSPIN3201 and 3202 are now back in the MCSDK 5.1.1 that is available for download.

Regards

Cedric

If you agree with my answer, please accept it by clicking on 'Accept as solution'."
Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards