2025-01-12 3:27 AM
Hi every one
I have defined a custom motor and inverter successfully.
Now I need to define custom features like a simple Digital output(LED for instance).
Is there any way?
or should I cut working on stmcubemx and continue coding after code generated by workbench.
in other words:
Is there any way to modify workbench generated .ioc file and again generate project file after editing it?
(for example after adding a digital output?)
Thanks a lot
Solved! Go to Solution.
2025-01-13 2:34 AM
Hello Carador,
After the .ioc generation via WorkBench, you are allowed to configure again your project using CubeMX to fit your application, and re-generate again without tampering with the motor control code. Obviously, this only works if you don't modify the Motor Control related configuration done by the Workbench.
2025-01-13 2:34 AM
Hello Carador,
After the .ioc generation via WorkBench, you are allowed to configure again your project using CubeMX to fit your application, and re-generate again without tampering with the motor control code. Obviously, this only works if you don't modify the Motor Control related configuration done by the Workbench.
2025-01-14 12:36 AM
Hi Dear Gael A
Thanks to your great response.
There is a little problem here:
I generate and compile V/F example without any problem.
Then I open Stm32Cubemx and with no modification again generate the code using it.
This time after compilation I face with this error:
fatal_error: arm_math.h No such file or directory
I know I may be able to dig the code and overcome this error but I think there is a bug in version 6.3.2 or I am making a mistake that is not clear to me.
would you please help me?
Thanks
2025-01-14 12:56 AM - edited 2025-01-14 1:04 AM
Hello Carador,
As you are using an example, the handling is a bit different. Let me ask a few questions :
First, what version of CubeMx are you using for code generation ?
Did you save the project in a different folder with CubeMx before re-generating ?
2025-01-14 1:07 AM
Hi again
I use version 1.17.0 of CubeMx and generated the code using latest version of firmware.
Yes, I saved example using save as and save it in another location with new project name.
No, I did not save it in another folder before regenerating it.
yours.
Carador
2025-01-14 1:22 AM
Hello again,
I think you are mixing up CubeMx and CubeIDE. Even though CubeMx has an integrated GUI inside CubeIDE, it is a different software that is responsible for code generation. Its latest version is 6.13. On the other hand, CubeIDE manages code display and debugging, and its latest version is 1.17.
I would like to know which CubeMx version you used for generation. You can see it just before generation via Workbench.
2025-01-14 1:27 AM
Sorry
Yes, I mixed up versions.
here is the correct ones:
STM32CubeIde Ver 1.17.0
STM32CubeMX Ver 6.13.0
with best wishes,
Carador
2025-01-14 2:35 AM
Dear Gael A
I compared 2 folder:
in Folder B the generated code using .ioc and STM32CubeMX,
one line is missing in .cproject
this is :
<listOptionValue builtIn="false" value="../../Drivers/CMSIS/DSP/Include"/>
it is in this section:
<option IS_BUILTIN_EMPTY="false" IS_VALUE_EMPTY="false" id="com.st.stm32cube.ide.mcu.gnu.managedbuild.tool.c.compiler.option.includepaths.1663155527" name="Include paths (-I)" superClass="com.st.stm32cube.ide.mcu.gnu.managedbuild.tool.c.compiler.option.includepaths" valueType="includePath">
When I added this line, problem solved.
I wish your team will ad this line in future releases or any solution, so we can generate code using STM32CubeMX without this modification.
After that I would like to open a more challenging discuss.
Thanking you in anticipation.
2025-01-14 9:06 AM
Dear Gael A
Thanks you a lot, Now I have no problem and feel free to edit just a line in .project, it is easy.
Thank you so much.
With best wishes,
Carador