cancel
Showing results for 
Search instead for 
Did you mean: 

Motor becomes unstable at 1200 RPM and stops with the P-NUCLEO-IHM001 Motor control Kit and Motor Control SDK 5.4.4 .

AKhar.3
Associate

I am using the P-NUCLEO-IHM001 motor development kit

Hardware:

Microcontroller Board: NUCLEO-F302R8

Driver Board: X-NUCLEO-IHM07M1

Motor: Bull-Running model BR2804-1700 kV

Software:

Keil uVision 5 IDE

ST Motor Control Workbench 5.4.4

Motor Control SDK 5.4.4

I am doing a hands-on activity on the P-NUCLEO-IHM001 Motor Control Kit. I generated the code using ST Motor Control Workbench and flashed the Microcontroller with the same code. But when I set the speed at 1200 RPM in Motor Control Workbench, the motor becomes unstable and stops. How can I run the motor at speeds less than 1200 RPM. Any help would be greatful. Thankyou in advance.

0693W000006GNQhQAO.jpgFig.1 Motor speed is is 3000RPM

0693W000006GNRGQA4.jpgFig 2. Error occurs when I set speed to 1200 RPM and motor stops

3 REPLIES 3
Laurent Ca...
Lead II

Dear @AKhar.3​ 

According to your description, you use SDK 5.4.4 and not 5.3 .

Therefor, I updated the title of your post.

Best regards

==

Laurent Ca.

Thank you for editing the title, Do you have any solution for the given problem?

Laurent Ca...
Lead II

The question has been set only to the "STM32 Motor Control" topic (the question is only about the STM32 MC SDK). 

Best regards