cancel
Showing results for 
Search instead for 
Did you mean: 

Missing library "TrajCtrl.h" when creating project on kit STEVAL-ETH001V1

phamtutailtvm
Associate

I bought the STEVAL-ETH001V1 kit on digikey. I also downloaded the firmware for the servo drive. However, when I build this project using keil c, the "TrajCtrl.h" library is missing and this library is not provided in the firmware.
I would like to ask where I can find this library or can someone help me?

2 REPLIES 2
GMA
ST Employee

Hello @phamtutailtvm,

Loading project on IAR, PositionDemo.c file, that uses TrajCtrl.h file, is not part of the project. Could you try without it?

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA

Why don't you provide that file in the firmware? I use Keil C to run and debug for my project. So i need that file to continue my project. 
If possible, can you provide me that file?