cancel
Showing results for 
Search instead for 
Did you mean: 

MCSDK 6.3 cannot find STM32CubeMX installed with STM32CubeIDE

gingerologist
Associate II

A standalone installation of STM32CubeMX could solve the problem. But I'm worried that if the version of the two mismatches there may be some potential problems in future, since STM32CubeIDE auto-updates frequently and the included STM32CubeMX may update automatically.

 

Is there any settings to make MCSDK using STM32CubeMX installed with STM32CubeIDE?

1 ACCEPTED SOLUTION

Accepted Solutions
AScha.3
Chief II

Hi,

>since STM32CubeIDE auto-updates frequently 

no - if you stop this, no update. (in Window-> Preferences )

AScha3_0-1721160145463.png

+ disable the "login" feature.

-> Try. As long, as you dont need new version, for new cpu or features, you can "fix" it to actual state.

AScha3_1-1721160568813.png

+

AScha3_2-1721160609092.png

 

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

2 REPLIES 2
AScha.3
Chief II

Hi,

>since STM32CubeIDE auto-updates frequently 

no - if you stop this, no update. (in Window-> Preferences )

AScha3_0-1721160145463.png

+ disable the "login" feature.

-> Try. As long, as you dont need new version, for new cpu or features, you can "fix" it to actual state.

AScha3_1-1721160568813.png

+

AScha3_2-1721160609092.png

 

If you feel a post has answered your question, please click "Accept as Solution".

Thank you for your advice.