cancel
Showing results for 
Search instead for 
Did you mean: 

MC workbench generation has errors.

dqsh06
Associate II

hello, 

now i am trying to use MC workbench 6.3.0 to generate a simple design, but there are errors.

the log is like below:

dqsh06_0-1720684006324.pngdqsh06_1-1720684113794.pngdqsh06_2-1720684138769.png

what is worry with MC workbench?  please help. 

thanks.

3 REPLIES 3
GMA
ST Employee

Hello @dqsh06,

The issue is already followed in this post.
As the project is fully generated, you can compile and use it.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA
dqsh06
Associate II

Hello GMA,

I have checked the post you mentioned, it seems the issue is still open, errors still occur.

but you said the project is fully generated, i can use it. so you mean the errors can be ignored , just use the codes, right?

i will try.

Thanks,

dqsh  

Hello @dqsh06,

Yes, issue is under investigation. Please ignore it for the moment and use generated project.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA