2025-01-16 7:25 PM
"I am currently using the STSPIN32G4 chip to design a motor drive controller with an external 6V supply for the gate driver. The DC bus voltage (VM) is selected to be 4V, which is less than 5.5V. When the motor speed is high, the gate driver triggers a reset. However, when the VM voltage is increased to 4.5V, the driver operates normally. What could be the possible reasons for this?