cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a problem with these conflicts?

TKara.2
Associate II

TKara2_0-1727205359974.pngTKara2_1-1727205368020.pngTKara2_2-1727205381799.pngTKara2_3-1727205389063.pngTKara2_4-1727205395368.png

Hi,

 Is there a problem with these conflicts? 

 

1 ACCEPTED SOLUTION

Accepted Solutions

Infact, if you are able to configure a pin, it should not have any problem. In case it will be the source of a problem, CubeMX will not let you set it.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
STTwo-32
ST Employee

Hello @TKara.2 

In fact those conflict means that some or all of the functions available in this IP can't be used for different reason such as Pin conflict with another API e.g if you have configured a pin for a Timer function and this button is the only one that can be used as DE for an USART interface. In this case this USART interface can't be used for RS485 mode (since it need to have a DE pin). The only solution is to disable the Timer implementation on this pin.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

"Would it cause any issues if one of the current sensing pins conflicts with the motor driving pins?

Infact, if you are able to configure a pin, it should not have any problem. In case it will be the source of a problem, CubeMX will not let you set it.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.