2020-04-21 10:18 AM
My computer crashed & I needed to reinstall all my tools on another system. Both are Windows 10 64x. I can't get the Motor Profiler 5.4.3 to connect on the new system. When I try to connect I get a message it can't find the MFC100.dll. I installed the Visual C++ 2010 redistributable and got the same results after rebooting. I uninstalled the 2010 redistributable and repeated with the 2013 version. Same results. The system connects fine with the Motor Control Workbench 5.4.3.
What's the secret sauce ??
2020-04-26 8:51 PM
I'll answer my own question after considerable debug.... The profiler is installed in the Program Filex(x86) folder; I think it's a 32-bit program. I installed both 32-bit and 64-bit Visual C++ 2010 Redistributable. So now mfc100.dll is available for both 32-bit & 64-bit. This seems to work now.
2021-06-21 10:31 PM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
2021-07-24 1:58 AM
Je confirme qu’il faut utiliser une version c++ 2010, pas la version 2015-2019