Hello,I need to profile a motor to be used in a drone. I can profile it sussefully without and also with propeller on, but wich is the correct way to profile it? And why?Thanks
I'm using ST motor profiler. The motor is a Protronik 2810, 1000KV, 25Apk, with a 3 cell battery (11.1V) and a 10x5 inches propeller (graupner e-prop).
Well, I solved my problems in two steps!My configuration is:B-G431B-ESC17 pole motor of 1000KV (Protronik DM2810-1000), rated for about 9800 RMP at 12V, 26.6A with a propeller 10x53 cells LIPO batteryFirst of all, I had to increase the Current Thresh...
Well,it's seem we have almost the same problems. When we try to reach full rpm we get an overcurrent fault, the motor brutally stop and consequently we get a speed feedback fault. I verified I have both fault at same time with the function MC_GetOccu...
Hello Sburc.1,Your description will surely help other peoples.What kind of motor are you using? What range of RPM?I'm using a 1000KV brushless with a propeller and a LIPO battery with 3 cells, but at high RPM I get a speed feedback fault and an over ...
Hello,Times ago I found under the folder of X-CUBE-MCSDK installation, you should find the source of a project that support PWM signal.I'll post more details tomorrow...