2018-04-16 5:47 AM
Hi folks !
while generating mcsdk files, I am getting this error which says that 'No STM32Cubemx version above 4.25.0 has been found' and Generation is not possible.
Could someone please help me get rid of this problem ?
thanks....
#sdk #stm32 #mc #cubemx #mcsdk #pmsm2018-04-19 12:53 AM
Hi,
Now, Motor control SDK depends on cubeMx to generate your project. You need to install it first.
You can find it here :
2018-04-19 7:40 PM
Hi dear Cedric,
Thanks for your reply.
I have already installed the latest version of cubemx. Even, I have uninstalled and installed both mc sdk 5.0.2 and cubemx a couple of times.However, the problem has not been solved yet.
Do you have another idea or suggestion ?
thanks a lot in advance....
2018-04-20 5:34 AM
2018-04-20 7:15 AM
Hi,
5.0.3 has been released and should fix your issue. Could you give it a try and let me know if it works.
Thanks
Cedric
2018-04-20 7:20 AM
Hi Cedric,
I have just downloaded and installed 5.0.3, but the problem is still there. Unfortunately, I can not generate the code for motor control.
I have removed and installed stm32cubemx, too. Nothing changed.
any idea ? And also I have tried these procedures on my 3 computers.
(in documantations, it is written that firstly, we need to install stm32cubemx and run at least once. I have done this as well.)
Thanks for your help Cedric....
2018-04-20 7:35 AM
That is the screenshot of the error. The only difference I see is that there are two same error messages instead of one compared to previous version of mcsdk.
2021-06-15 1:34 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards