cancel
Showing results for 
Search instead for 
Did you mean: 

I'm using EVSPIN32F0601S3 to run a BLDC motor. The max RPM of the motor is 18,000. Whereas I could go up to a maximum of only 15,000 RPM.

Manoj.M
Associate II

Any FAE from India (Bangalore office) please guide for resolving it.

4 REPLIES 4
Javier1
Principal

If i were you i would post more info about your motor

we dont need to firmware by ourselves, lets talk
Manoj.M
Associate II

Hello,

Thanks for the info, attached the motor specs.

0693W00000aIY57QAG.png

How much current are you measuring when reaching 15000rpm?

we dont need to firmware by ourselves, lets talk
Manoj.M
Associate II

Less than 1.2A in the motor phase when measured in AC Fluke clamp meter.

I have tuned the current regulator PI values by using the step function in the monitor.

And after a few minutes of continuous running(no parameter changed), the motor stalls and gives a speed feedback error in the monitor.