2020-07-20 6:58 AM
only can't write interrupt command for working
my board with stm32f103
this is a source code
attachInterrupt need to convert for this platform this is written no right
thnak's
i keep file in here
2020-09-14 1:39 AM
Dear MAvet.1
Do you have still this problem to solve?
Best regards
Laurent Ca...
2020-09-14 3:00 AM
Yes of course
2020-10-20 8:03 AM
Dear @MAvet.1
Could you give more details to the STM32 Community about the material you use (HW and SW, CPU(s), tools and versions, board(s), motor(s) and so on)?
And more especially did you use MC tools (such as MC_suite, MC-Motor Profile, MC-SDK, MC-workbench, and so on)?
Best regards
Laurent Ca...
2020-10-26 2:58 AM
Dear @MAvet.1
Any news?
Best regards
Laurent Ca...
2020-11-02 12:33 AM
Dear @MAvet.1
As you do not answer, I guess you don't have to solve this problem anymore, therefore I consider this thread closed.
If not, feel free to reopen it by posting a new answer.
Best regards
Laurent Ca...