cancel
Showing results for 
Search instead for 
Did you mean: 

I am using STM32H743VITx controller and i want to interface it with a BLDC motor.

SVerm.6
Associate

While debugging the code everything works fine until i give command to start the motor i.e the moment i generate PWM and motor starts rotating, Cube IDE generates a message that the "target is not responding".

Also I've made sure that SWDIO, SWCLK, and SWO pins are correctly mapped on the controller.

0 REPLIES 0