cancel
Showing results for 
Search instead for 
Did you mean: 

how to use Motor Control workbench 5.y.4 , Using example project update motor and generate code?

MMand.3
Associate

I am trying to evaluate STSPIN32F0251S1 , 

My requirement is use 6 steps ( trapezoidal ) implementation , 

I tried to use example project from motor control workbench 5.Y.4 

[EVSPIN32F0251S1] + [Shinano LA052-080E3NL1] HW setup using 

 * the Six-Step algorithm Voltage modes and Sensorless

software packages

  • STM32CubeMX v6.4.0
  • STM32Cube_FW_F0_V1.11.2

when i tried update motor parameter and Generate code is show some error (image attached) .

if choose the only update option then code generates but motor parameter remain same.

Need some help

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0