cancel
Showing results for 
Search instead for 
Did you mean: 

How to use MC Workbench to generate project for STM32G474 in LQFP64 package?

Larry Lukis
Associate II

I see that 128 pin package is supported even though it is a non-stocked item at Digikey. I can build a project for that package, but I need to build for the 64 pin package. How can I do that?

1 REPLY 1
Laurent Ca...
Lead II

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards