cancel
Showing results for 
Search instead for 
Did you mean: 

How to generate motor *.stmcx file from *.xml file

BTrem.1
Senior II

This is a basic question but has me stumped. I have an existing motor project with a *.stmcx file. I generated a new *.xml file for the motor using the profiler. How do I get the *.xml file converted over to a new *.stmcx file? I can load the existing project in the Motor Control Workbench but it doesn't give an option to load a new motor file .....

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Laurent Ca...
Lead II

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards