cancel
Showing results for 
Search instead for 
Did you mean: 

How to use inline phase shunts with ST MC Workbench code?

Liann1
Associate

Hi, I'm developing a board to control motors using FOC. For this, I will use the MC workbench tool to generate the code. However, when I describe the hardware in the shunt resistors section, there is no "in-line" option, only the low-side option, but my board only has them in-line and I can no longer modify it. What can I do in the code to be able to use the shunt resistors in this way?

0 REPLIES 0