2022-02-25 2:09 PM
I use STM32CubeIDE (1.5.0) as a toolchain without a current CubeMx file. What is the means of upgrading motor drivers from 5.4.4 to 5.Y.4?
I have done the basic install of 5.Y.4 under folder C:\Program Files (x86)\STMicroelectronics but in my CubeIDE project the drivers are duplicated under folder:
C:\Users\Brian\ST_workspaces\Bitbucket - repo -v03.10.02 - New_Filter\cascade_pfd\Prysm_Test_Board_LL
I tried replacing the 5.4.4 folder in my project with the 5.Y.4 folder but get a build error.
I then edited the path in Project//Properties/Paths to the new folder location of 5,Y.4..
Are there any notes somewhere to go through the steps of upgrading the motor drivers?
Thanks,
Brian