STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1717 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4870 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9550 Views
  • 5 replies
  • 3 kudos

MCSDK 6 board config

Using the SDK I am basing a new system on the EVSPIN32G4. After selecting the inverter, and motor, I am then taken into the parameter configuration of the motor driver.According to the boards manager the EVSPIN32G4 has multiple configurations availab...

Motor control fails after motor stop

I am using an e-bike motor 48V350W with an EVALSTDRIVE101 3Sh and NUCleo F401REboard to do some tests. The motor only starts the first time I press start and then if I stop it doesn't resume rotation unless I restart the Nucleo board. I analyzed the...

MLasc.1 by Associate
  • 1388 Views
  • 1 replies
  • 0 kudos

Resolved! using stm32wl55ccu to drive 3 phase bldc

Hi ,I am using stm32wl55ccu 48 pin QFN MCU to drive a 3 phase brushless motor using 3-phase complementary PWM output signals using TIMER 1. I have seen at the datasheet that this 48 QFN package is missing the complementary output of TIMER1 ,Channel 3...

YY55 by Associate
  • 1767 Views
  • 1 replies
  • 1 kudos