cancel
Showing results for 
Search instead for 
Did you mean: 

how to create the PFC feature code with STEVAL-CTM010V1 board

Jameszhan
Associate II

i got a STEVAL-CTM010V1 board and installed the SDK(5.4.4 full),after that i created a project base on example(STEVAL-CTM010V1 dual drive with PFC,see pic_1),but the example does not enable the PFC feature(see pic_2),so if we want to use the PFC feature on CTM010V1 board ,what should we do ?

5 REPLIES 5
Jameszhan
Associate II

@Claire OKU (ST Employee)​ 

Jameszhan
Associate II

i found a tips to fix this issue,just need to modify the config.xml file(C:\Program Files (x86)\STMicroelectronics\MC_SDK_5.4.4\Utilities\PC_Software\STMCWB\assets\xml).

hence,if you remove the warning ,you can config the PFC feature on WB.

.

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards

Hi Jameszhan,

Is it safe doing that?

Best Regards,

Rado

Lmazz.1
Associate II

Any solution to this ?

many thanks