2016-11-09 7:41 AM
Hello everyone.
Recently I started to create a project to make control of a BLDC engine.I used, until now, the compiler eclipse AC6. I have read here, in the forum, that some people are using the SDK with AC6.Can someone explain the procedure, please?Thank you very much. #ac6 #foc-sdk2017-01-10 12:53 AM
Hello
Martins.David
,You can refer to openSTM32 website.
Following link details how to install eclipse plugins to be able to compile CubeMX generated code:
http://www.openstmorg/Installing+System+Workbench+for+STM32+from+Eclipse?structure=Documentation
hope it answer your question.
If I missunderstood it, could you please elaborate a bit what you are trying to achive ?
Thanks in advance.
KR
Sirma
2021-06-15 4:36 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards