2016-12-13 6:09 PM
I noticed the function description of the PI_GetDefaultKI and the PI_GetKI are same in FW API description. What is the difference between them?
I can't understand PI_
SetIntegralTerm. the description is so vague.
Can someone explain something , please?
thanks.
#library #foc-mdk-4.32021-06-15 12:21 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards