2017-03-09 02:11 AM
Hello.
I'm using the FOC SDK (v4.3) with a incremental encoder.
I need to know what, in practice, means the angle placed on 'alignment electrical angle'.https://spostimg.org/y32f6ts1h/Capturar.png
I'm having some problems because I'm using a BLDC motorand at low speed the motorhas a lot of cogging.
Do you have any suggestions to solve this?Throughout the range of 500->4000RPM everything works well! Below 500RPM it is difficult to maintain control. I'm using an encoder with 500ppr on a motor with 2 pairs of poles.
Do you have any idea?
Thank you. encoder bldc foc-sdk angle2017-03-15 11:27 AM
Someone can help me?
Why can not I get a perfect spin below 500RPM?
I am using an incremental encoder of 500ppr. The control has good feedback ...2021-06-15 01:59 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards
2021-06-15 02:00 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards