2016-12-28 6:38 AM
Hi'
I have a strange problem.
I use Win 10, and Keil MDK-ARM 5.11 version
I installed the newest 4.3 PMSM foc environment, and usb driver, and firmwares.
My board is
NUCLEO
-
F303K8 and x-nucleo-ihm07m1 expansion board
I can use the motor profiler, and the workbatch runs correctly.
The all kind of link works/st link/virtual com port...
I compiled the code in the keil5 without error.
But when i press the button to set the (st-link)debug link on the wizard screen,♯ the MDK-ARM is collapsed.
All other case i can set the link (example codes, own codes, different nucleo boards) except when i use 4.3 PMSM foc.
I tried to set the link with another boards but in the all cases collapsed the MDK-ARM. I think my board work well, so i have got any software/settings problem
I can do all this settings without problem in the 4.2 PMSM foc.
Can anybody help me what is my mistake?
#stm32-pmsm-foc-sdk2017-01-07 11:58 AM
The problem solved.
Downgrade win10 to win7 and upgrade the Mkd_arm 5.11 to 5.22 version.
2021-06-15 1:59 AM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards