2018-04-03 02:38 AM
I would like to use the serial protocol to communicate with the FOC 4.3. I need to have a feedback of the motor status (overcurrent fault..). Two readable registers (status ans flags) are described in the user manual (UM1052 p164) but I can't find any precise description of each bit of this registers.
Thanks by advance for your help.2021-06-27 10:45 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards