cancel
Showing results for 
Search instead for 
Did you mean: 

Evaluating Motor Control using AC6 Workbench for STM32

jorge2
Associate II
Posted on April 20, 2016 at 19:52

Hello, I am trying to evaluate motor control firmware with AC6 Workbench. I am looking at the STM32 PMSM FOC SDK 4.2, Hands-on workshop with hardware tools, Rev 1.5, and it only supports Keil and IAR. Is there a version for AC6 Workbench?

Thanks.

2 REPLIES 2
Gigi
ST Employee
Posted on April 21, 2016 at 08:31

Ciao

No I'm sorry. At the moment the workspaces for AC6 is not provided with the last release of the MC FOC Lib.

Ciao

Gigi

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards