cancel
Showing results for 
Search instead for 
Did you mean: 

Current surge with hall sensor at engine start

Oli49
Associate II

Hello Everybody,

MCSDK : 6.3.2
CubeMX: 6.3.2
Workbench : 6.3.2
Cube IDE : 1.18.1
Hardware : Custom but based on EVLDRIVE101-HPD
Motor : PMSM 28V - 2 pole pairs - Rmp = 14K - rated current = 13A - Primary sensor : Hall, Secondary sensor Observer+PLL (sensor less)

At power up, after a delay, the motor start with hall sensor.
When motor control switch to RUN, there is current surge, limited by my power supply (15A), during 100ms. (PWM > 90%).
Is it to align the rotor ???
If i use FOC as primary sensor, you can limit the current but not if i use Hall sensor as primary sensor.

I have change IQMAX_A, NOMINAL_CURRENT_A and ID_DEMAG_A at different value, but i has no effect.

What can un do to limit this current to 3/4A during this phase ?

After this surge, the motor works well.

(Green : rpm, Yellow : power supply voltage, Blue : Power supply current, Purple : W current)

5 REPLIES 5
STuser2
Senior III

Can you try with MCSDK 6.4.1 i think there are some improvements or changes, this is my suggestion.

Oli49
Associate II

MCSDK 6.4.0 and 6.4.1 doesn't work !!


why what is the reason?

Oli49
Associate II

For example, with 6.3.2 at 3500rpm, the motor current is sinusoidal, the power supply current is 0.15A@28V.
with 6.4.x the motor current is erractic, the power supply current is 4.5A@28V, and the motor is noisy.
I don't know what the problem is, and i don't have time to waste debugging this MC SDK version.

Hello @Oli49,

A test has been conducted on the ST side with MCSDK6.4.1 and Hall without any issues.
Using Primary sensor: Observer + PLL (sensorless) and Secondary sensor: Hall, did you plot both EL_ANGLE signals to verify that they are aligned?

 

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA