cancel
Showing results for 
Search instead for 
Did you mean: 

Can the STSPIN32G4 be used to drive a brushed motor?

Shane Kent
Associate II

Hello -

I'm wondering if the STSPIN32G4 can be utilized to drive a brushed motor rather than a three-phase brushless motor that it is marketed for. Alternatively, are there any chips within STMicro that are meant for brushed motors that have a combined MCU and gate driver like the STSPIN32G4?

Thank you!

-Shane

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @Shane Kent​, to the community!

The STSPIN32s are particularly advantageous when all the resources they contain are used, which is the case with three-phase BLDC motors. But of course, all STSPIN32 can also be used for brushed motors, but then one half bridge is unused.

If necessary, the nearest distributor or ST office can help you with the design.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @Shane Kent​, to the community!

The STSPIN32s are particularly advantageous when all the resources they contain are used, which is the case with three-phase BLDC motors. But of course, all STSPIN32 can also be used for brushed motors, but then one half bridge is unused.

If necessary, the nearest distributor or ST office can help you with the design.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.