2023-06-17 09:53 AM - last edited on 2023-06-17 02:51 PM by Amel NASRI
Hello. I would like to design a bldc motor controller using stm32G4 series. I recently ordered stm32g431rbt6 because of the on chip opamps and dacs. Also in the datasheet it states that there are timers for advanced motor control. I am seeking assistance on where to start with the motor controller design and what tools from STM I can use to achieve my goal. The project has a limited deadline and I would like support on the controller design. The motor I will be using is a hub motor. I would also appreciate any other information concerning microcontroller selection and whether I should use a different microcontroller. Thanks.
2023-06-17 09:15 PM
Hi,
One can start here:
See more: https://www.youtube.com/@stmicroelectronics/search?query=Motor%20control