2020-07-28 08:09 PM
Hi,
I tried using the motor profiler with B-G431B-ESC1 for an A2212/6T 2200kv motor but it just won't run.
The profiler tries to move the motor and it sound's like it is trying to move, but never really rotates. After some time it says the profiler is optimized for motors with bigger resistance and inductance.
Manually measuring the resistance shows a value around 0.5 ohms which seems to be in spec according to the profiler warning.
Should I be doing something differently? or is it just not compatible with these motors?
Best,
David
2021-06-27 09:33 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards