cancel
Showing results for 
Search instead for 
Did you mean: 

B-G431-ESC1 develoopement kit Electrical Speed control example generated code?

N_1
Associate II

Hy everyone,

The electrical speed control example code works the following for me:

Starts the motor with PWM, and then stops it after it reached the maximum speed. It turns off the PWM signal.

I tried to modify the code to just start the motor but every time it stops. Could you help me what function should or shouldnt I call? The state machine a bit comlicated for me, But even if I do not invite any of the stop functions, it still stops. Thank you!

2 REPLIES 2
Laurent Ca...
Lead II

Dear N

Do you have still this problem to solve?

Best regards

Laurent Ca...

Dear N

OK. I consider this post closed.

Do not hesitate to answer if it is not.

Best regards

Laurent Ca...