STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1726 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4875 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9572 Views
  • 5 replies
  • 3 kudos

Speed feedback problem during Motor profiling

Posted on May 19, 2017 at 09:13I try to run the motor profiler with my custom prototype SM-PSMS motor. In this moments I hold the motor in a big vise, so the motor is impossible to move when start the current. When I run the motor profiling usually ...

manuele by Associate
  • 1072 Views
  • 1 replies
  • 0 kudos

Do anybody have any idea on what sequence does ST Motor Profiler follow to measure inductance ? How accurate it is ?

Posted on June 12, 2017 at 04:29The motor profiler starts profiling starts to measure the motor parameters like R,L ,Kb and other mechanical parameters but every time i use the values are different from physical measurements  which gives me a confus...

FOC 4.3 + F303 + GCC + Errors

Posted on June 26, 2017 at 06:25I use FOC4.3 for my project based on nucleo303+IHM07M1, with GCC compiler.I found a few errors in the library. May be it can be useful for a MC team or community.1. Invalid ifdef for CCRAM attributes. GCC compiler not...

MCSDK & Motor Profiler with low RPM BLDC motor

Posted on May 01, 2018 at 22:23Hello,I am trying to use the MCSDK to control a 250W BLDC motor. Here the the specification.Electrical 36V nom, 7 amps max, 10 pole pairs.Mechanical ~ 8 N.m, and no more than 300 RPM.I am using the F302R8 and IHM08M1 i...

0690X0000060ArYQAU.png

Any example on how to use MCSDK 5.0?

Posted on May 15, 2018 at 03:11The 5.0 version use commands like 'bool MC_StartMotor1(void);' instead of the old 4.3 'bool MCI_StartMotor(CMCI this);' This api change is documented in AN5143 rev 2.A google search on MC_StartMotor1 gives one hit - in...

Motor Profiler fails

Posted on May 21, 2018 at 16:58My end aim is to use #Motor #profiler to workout my motor parameters. I have #nucleo-F302R8 and #X-nucleo-IHM08M1 boards.I selected these two in Profiler, Connected My motor and Hall devices, Entered 4 Pole pairs and m...

dsystem by Associate II
  • 910 Views
  • 1 replies
  • 0 kudos

How to use Motor Profiler with STEVAL-ESC001V1

Posted on June 03, 2018 at 09:43I am trying to use the STEVAL-ESC001V1 with the motor profiling tool but I can't get the motor profiler to connect to the controller. I am using a ST-LINK/V2 with the STSW-LINK009 driver on Win7. I am able to connect ...