2019-12-16 12:37 AM
Hy everyone,
The electrical speed control example code works the following for me:
Starts the motor with PWM, and then stops it after it reached the maximum speed. It turns off the PWM signal.
I tried to modify the code to just start the motor but every time it stops. Could you help me what function should or shouldnt I call? The state machine a bit comlicated for me, But even if I do not invite any of the stop functions, it still stops. Thank you!
2020-09-10 11:24 PM
Dear N
Do you have still this problem to solve?
Best regards
Laurent Ca...
2020-09-22 7:49 AM
Dear N
OK. I consider this post closed.
Do not hesitate to answer if it is not.
Best regards
Laurent Ca...