cancel
Showing results for 
Search instead for 
Did you mean: 

AS5047P can connect IHM07M1 using motor control workbench

bRun.1
Associate

I have a X-NUCLEO-IHM07M1 and a BLDC motor.

BLDC motor have a encoder AS5047P, ABI interface.

first, I just connect encoder pin:

A to PA10;

B to B3;

I to B10;

secondly, change the speed sensor to quadrature encoder, and generate the code;

i just get a error:

"Main speed sensor is set to the Quadrature Encoder sensor, but the motor doesn't support it"

is X-NUCLEO-IHM07M can not support AS5047P?

this is 5047p infomation:

https://ams.com/en/as5047p

2 REPLIES 2
bRun.1
Associate

i got it.

what was it?