2024-07-26 06:32 AM
Hello everyone,
I am generating the observer for an Induction motor with a FOC loop. However, I am unsure about the appropriate values for the observer parameters (see image below). I've read that the LSO Gain should be between 1 and 1.5, but I'm uncertain about the suitable ranges for Kp and Ki or the ideal bandwidth for using the Auto Calculate function.
I am working with an induction motor with the following characteristics:
There are some considerations that I should take into account in order to choose LSO Gain, Kp, and Ki, or what are the suggested ranges.
More details about my setup :
[VERSION]: MCSDK 6.3.0 & 6.2.1
[TOOL]: MC WB