cancel
Showing results for 
Search instead for 
Did you mean: 

I am having an issue in the code generated from X-CUBE-AI library. The C generated code for my tflite model (called network) is giving following error: /X-CUBE-AI/App/network.h:40:3: error: invalid initializer

BFaru.1
Associate II

The error is in the network.c code file generated by the X-CUBE-AI library. I have chosen "Not Selected" option in drop down option for X-CUBE-AI. The code below is giving the error as mentioned:

0693W00000bhR9nQAE.png

2 REPLIES 2
fauvarque.daniel
ST Employee

This macro is deprecated and not used in the generated code normally

Regards


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

Is there a way around it?​