Skip to main content
Associate II
June 15, 2024
Solved

Unable to get DMA transfer complete to trigger

  • June 15, 2024
  • 4 replies
  • 2580 views

I'm using TIM1 to write a DMA buffer to the built-in LED. I'm trying to get the Transfer Complete callback to trigger. I've tried setting hdma->XferCpltCallback to a function. I suspect there is an interrupt enable flag I need to set and probably clear.

Here's my main.c:

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
#include "dma.h"
#include "tim.h"
#include "usart.h"
#include "gpio.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <stdio.h>
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */

/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/

/* USER CODE BEGIN PV */
// TIM_HandleTypeDef htim1;
// DMA_HandleTypeDef hdma_tim1_up;

// UART_HandleTypeDef huart2;
/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
/* USER CODE BEGIN PFP */
// void SystemClock_Config(void);
// void MX_GPIO_Init(void);
// void MX_USART2_UART_Init(void);
// void MX_DMA_Init(void);
// void MX_TIM2_Init(void);
#define PUTCHAR_PROTOTYPE int __io_putchar(int ch)
/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
// void dmaComplete(DMA_HandleTypeDef *_hdma){
// UNUSED(_hdma);
// printf("dma done\n");
// }

void HAL_TIM_PWM_PulseFinishedCallback(TIM_HandleTypeDef *htim)
{
 printf("DMA done\n");
}

void HAL_TIM_PWM_PulseFinishedHalfCpltCallback(TIM_HandleTypeDef *htim)
{
 printf("DMA half done\n");
}

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_TIM1_Init();
 MX_USART2_UART_Init();
 /* USER CODE BEGIN 2 */
 uint32_t clockedData[13];
 uint32_t count=0;
 for(int i=0;i<13;i++)
	 clockedData[i]=0;
 // the clockedData goes straight to the BSRR register
 // [31 ... 16] are reset bits corresponding to Ports [15 ... 0]
 // [15 ... 0] are set bits corresponding to Ports [15 ... 0]
 // if a reset bit is set, the GPIO port will be set LOW
 // if a set bit is set, the GPIO port will be set HIGH
 clockedData[ 0] = 0x00000008; // LED on
 clockedData[ 1] = 0x00080000; // LED off
 clockedData[ 6] = 0x00000008; // LED on
 clockedData[12] = 0x00080000; // LED off

 // DMA, circular memory-to-peripheral mode, full word (32 bit) transfer
 HAL_DMA_Start(&hdma_tim1_up, (uint32_t)clockedData, (uint32_t)&(GPIOB->BSRR), 13);
 HAL_TIM_Base_Start(&htim1);
 HAL_TIM_OC_Start(&htim1, TIM_CHANNEL_1);

 TIM1->DIER |= (1 << 8); // set UDE bit (update dma request enable)

 // HAL_DMA_RegisterCallback(&hdma_tim1_up, HAL_DMA_XFER_CPLT_CB_ID,&dmaComplete);

 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
 /* USER CODE END WHILE */
 printf("\r\nTimer DMA Test %d", count);
 count++;
 // HAL_GPIO_TogglePin (GPIOB, GPIO_PIN_3);
 HAL_Delay(1000);
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure LSE Drive Capability
 */
 HAL_PWR_EnableBkUpAccess();
 __HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSE|RCC_OSCILLATORTYPE_MSI;
 RCC_OscInitStruct.LSEState = RCC_LSE_ON;
 RCC_OscInitStruct.MSIState = RCC_MSI_ON;
 RCC_OscInitStruct.MSICalibrationValue = 0;
 RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI;
 RCC_OscInitStruct.PLL.PLLM = 1;
 RCC_OscInitStruct.PLL.PLLN = 16;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7;
 RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
 RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK)
 {
 Error_Handler();
 }

 /** Enable MSI Auto calibration
 */
 HAL_RCCEx_EnableMSIPLLMode();
}

/* USER CODE BEGIN 4 */
/**
 * @brief Retargets the C library printf function to the USART.
 * None
 * @retval None
 */
PUTCHAR_PROTOTYPE
{
 /* Place your implementation of fputc here */
 /* e.g. write a character to the USART1 and Loop until the end of transmission */
 HAL_UART_Transmit(&huart2, (uint8_t *)&ch, 1, 0xFFFF);

 return ch;
}
/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}

#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * @PAram file: pointer to the source file name
 * @PAram line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

 

Here's tim.c where the DMA is setup and I assign the callback:

 

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file tim.c
 * @brief This file provides code for the configuration
 * of the TIM instances.
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2024 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "tim.h"

/* USER CODE BEGIN 0 */
#include <stdio.h>
void dmaDone( DMA_HandleTypeDef * hdma){
 printf("DMA DONE\r\n");
};
/* USER CODE END 0 */

TIM_HandleTypeDef htim1;
DMA_HandleTypeDef hdma_tim1_up;

/* TIM1 init function */
void MX_TIM1_Init(void)
{

 /* USER CODE BEGIN TIM1_Init 0 */

 /* USER CODE END TIM1_Init 0 */

 TIM_ClockConfigTypeDef sClockSourceConfig = {0};
 TIM_MasterConfigTypeDef sMasterConfig = {0};

 /* USER CODE BEGIN TIM1_Init 1 */

 /* USER CODE END TIM1_Init 1 */
 htim1.Instance = TIM1;
 htim1.Init.Prescaler = 1000;
 htim1.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim1.Init.Period = 4000;
 htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim1.Init.RepetitionCounter = 0;
 htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim1) != HAL_OK)
 {
 Error_Handler();
 }
 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
 if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
 sMasterConfig.MasterOutputTrigger2 = TIM_TRGO2_RESET;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM1_Init 2 */

 /* USER CODE END TIM1_Init 2 */

}

void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* tim_baseHandle)
{

 if(tim_baseHandle->Instance==TIM1)
 {
 /* USER CODE BEGIN TIM1_MspInit 0 */

 /* USER CODE END TIM1_MspInit 0 */
 /* TIM1 clock enable */
 __HAL_RCC_TIM1_CLK_ENABLE();

 /* TIM1 DMA Init */
 /* TIM1_UP Init */
 hdma_tim1_up.Instance = DMA1_Channel6;
 hdma_tim1_up.Init.Request = DMA_REQUEST_7;
 hdma_tim1_up.Init.Direction = DMA_MEMORY_TO_PERIPH;
 hdma_tim1_up.Init.PeriphInc = DMA_PINC_DISABLE;
 hdma_tim1_up.Init.MemInc = DMA_MINC_ENABLE;
 hdma_tim1_up.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD;
 hdma_tim1_up.Init.MemDataAlignment = DMA_MDATAALIGN_WORD;
 hdma_tim1_up.Init.Mode = DMA_CIRCULAR;// DMA_NORMAL or DMA_CIRCULAR
 hdma_tim1_up.Init.Priority = DMA_PRIORITY_LOW;
 if (HAL_DMA_Init(&hdma_tim1_up) != HAL_OK)
 {
 Error_Handler();
 }

 __HAL_LINKDMA(tim_baseHandle,hdma[TIM_DMA_ID_UPDATE],hdma_tim1_up);

 /* USER CODE BEGIN TIM1_MspInit 1 */
 hdma_tim1_up.XferCpltCallback = &dmaDone;
 /* USER CODE END TIM1_MspInit 1 */
 }
}

void HAL_TIM_Base_MspDeInit(TIM_HandleTypeDef* tim_baseHandle)
{

 if(tim_baseHandle->Instance==TIM1)
 {
 /* USER CODE BEGIN TIM1_MspDeInit 0 */

 /* USER CODE END TIM1_MspDeInit 0 */
 /* Peripheral clock disable */
 __HAL_RCC_TIM1_CLK_DISABLE();

 /* TIM1 DMA DeInit */
 HAL_DMA_DeInit(tim_baseHandle->hdma[TIM_DMA_ID_UPDATE]);
 /* USER CODE BEGIN TIM1_MspDeInit 1 */

 /* USER CODE END TIM1_MspDeInit 1 */
 }
}

/* USER CODE BEGIN 1 */

/* USER CODE END 1 */

 

This topic has been closed for replies.
Best answer by mleo2

I needed to use HAL_DMA_Start_IT(). This starts the DMA with interrupts enabled.

Is there someplace that has all this stuff documented? I found this by going through the source code.

4 replies

BarryWhit
Lead
June 15, 2024

Did you remember to enable the DMA interrupt under the NVIC (Interrupt controller) peripheral in the CubeMX UI?

"- If someone's post helped resolve your issue, please thank them by clicking ""Accept as Solution"".- Please post an update with details once you've solved your issue. Your experience may help others."
mleo2AuthorBest answer
Associate II
June 15, 2024

I needed to use HAL_DMA_Start_IT(). This starts the DMA with interrupts enabled.

Is there someplace that has all this stuff documented? I found this by going through the source code.

mleo2Author
Associate II
June 15, 2024

Yes I did.

 

BarryWhit
Lead
June 15, 2024

> Is there someplace that has all this stuff documented? 

 

The HAL API follows a naming convention. Once you've used it for a while you know which function to call.

There's also a reference manual for the HAL for each family chip. For the G431 it's UM2570, for example.

 

"- If someone's post helped resolve your issue, please thank them by clicking ""Accept as Solution"".- Please post an update with details once you've solved your issue. Your experience may help others."