2024-06-14 10:17 PM
Hello,
I am working with STEVAL-SPIN3202 to develop motor control solution. I am using the Motor Control Workbench 6.2.1.
I could generate the project using the workbench, however when i Connect the evaluation board, window with FAIL.txt opens which reads "The interface firmware FAILED to reset/halt the target MCU".
Thus I am not able to connect to the board. I have tried connecting to the board using ST-Link Utility, however it gives the error message "Can not connect to target".
I have tried some of the solution mentioned on the forum but the issue still persist.
Please guide me so that i can get my motor running.
Solved! Go to Solution.
2024-06-15 01:51 AM
To the board...see manual:
2024-06-14 11:48 PM
Hi,
ST-Link Utility is old, deprecated. Dont use this .
So try with CubeProgrammer , connect "under reset" or "software reset" .
2024-06-15 12:03 AM
Hi,
Thank you for your reply. Tried with CubeProgrammer. Still no luck. It throws below error and when the board is connected FAIL.txt is still generated.
2024-06-15 12:29 AM
Hi,
"no target found" is just info: cannot connect...
So show, what CubeProgrammer shows...target voltage...etc.
so:
2024-06-15 12:36 AM
Below is what the CubeProgrammer is showing. If i chose Reset mode as Software reset, then also after pressing connect it automatically changes to hardware reset.
2024-06-15 12:45 AM
Ok,
now we see : target voltage 0,46V . This cpu cannot work... 🙂
Give it some power , 3v3 ; then check again.
(Maybe check jumper settings on board, see manual. Or need connect power supply...)
2024-06-15 12:51 AM
ok. where exactly is this voltage? and where do i need to give power supply?
2024-06-15 01:51 AM
To the board...see manual:
2024-06-15 07:35 AM
Thanks for help. It worked. I was under impression that MCU is supplied by USB. However, it was clear once i checked schematic. Thanks again.