cancel
Showing results for 
Search instead for 
Did you mean: 

x-cube EEPROM failing at EE_Init between step 3 and step 4

MAlam.3
Associate II

Two of my MCUs are halting in same problem after running for about a year. There have not been many writes/cycles as I have a erase cycle counter which shows 27 so its not wear out problem. The EE_Init function gets stuck at step 4 and returns with  EE_WRITE_ERROR. Here is the page situation. I use page 2 and 3 of second bank. Page 2 is in state RECEIVE (aaaa, ffff, ffff, ffff), the page is otherwise empty. Page 3 is in state ERASING (aaaa, aaaa, ffff, aaaa) and the page is full with data. The problem is already found in step 3 (pagestate = STATE_CORRUPTED),  where it checks that page 2 is RECEIVE but page 3 is not ERASED. The code however does not do anything about it. It only deals with the case if (pagestate = STATE_RELIABLE). Recovery transfer occurs in step 3 only for reliable page state . Therfore in step 4, there is no active page, no valid page and finally the function exits with EE_WRITE_ERROR

Here are the contents of page 2 starting at 0x08041000:

MAlam3_0-1748874300028.png

Here are the contents of page 3 starting at 0x08041800:

MAlam3_1-1748874365712.png

Can someone help me out with this?

 

3 REPLIES 3
Maxime_MARCHETTO
ST Employee

Hello @MAlam.3,

This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.

Best regards,
Maxime


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
MAlam.3
Associate II

Hi Maxime,

Thanks for your reply. Yesterday I already posted this to ST online support forum. It seems Tobias Puetz and Bertrand Pineau have been assigned to the case and they are probably looking itno it.

I was thinking to do it when ST support has provided a solution, then I would post the solution here as well and mark that as a reply so that others can also benefit from it.