cancel
Showing results for 
Search instead for 
Did you mean: 

Why stm32h743 pc1 can not set output speed to very high in cubmex

Yi Zhou
Associate III
Posted on July 01, 2018 at 15:42

Hi all:

    I using cubemx to config stm32h743 eth, why pc1 can not set output speed to very high, the pc1 can only select low, not like other pins.

0690X0000060C86QAE.png

Thanks. 

#stm32h7-ethernet
2 REPLIES 2
Posted on July 01, 2018 at 17:00

Doesn't MDC clock at 2.5 MHz max, what would be the value of aggressively slewing it other than generating unnecessary ringing and noise?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on July 04, 2018 at 13:51

Thanks Clive Two.Zero.