cancel
Showing results for 
Search instead for 
Did you mean: 

Which TCP/IP stack ST recommends to use with the STM32H7xx MCU lineup.

FB__1
Associate II

I have the options for :

  • FreeRTOS_Plus_TCP
  • lwIP 2.1.3 (recommended to upgrade to this based on the official website)
  • lwIP 2.1.2 (comes with the CUBEIDE).

I need a robust and stable stack.

1 ACCEPTED SOLUTION

Accepted Solutions
KDJEM.1
ST Employee

Hello @FB__1​ and welcome to the Community :) ,

Based on this discussion, the LwIP 2.1.3 isn't supported with STM32CubeIDE.

For that, it is recommended to still with LwIP 2.1.2 or to switch to X-CUBE-AZRTOS-H7.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
KDJEM.1
ST Employee

Hello @FB__1​ and welcome to the Community :) ,

Based on this discussion, the LwIP 2.1.3 isn't supported with STM32CubeIDE.

For that, it is recommended to still with LwIP 2.1.2 or to switch to X-CUBE-AZRTOS-H7.

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

LCE
Principal II

It's quite simple to update to LwIP 2.1.3 manually.

FB__1
Associate II

Thanks for the answers :)

Piranha
Chief II

> I need a robust and stable stack.

Then you cannot use the HAL/Cube broken bloatware anyway...

https://community.st.com/s/question/0D50X0000BOtfhnSQB/how-to-make-ethernet-and-lwip-working-on-stm32