2021-01-20 07:08 AM
Hi
I am developing the project with STM32F746 (STMCUBE IDE)
sending the data to the server . want to use WEBSOCKET protocol to do this
Is there any Library with example for WEBSOCKET with LWIP in STM32
Solved! Go to Solution.
2021-01-29 12:11 AM
Hello @sunil and welcome to the STM32 Community 😊,
Have a look to the LwIP example under STM32CubeF7 MCU package, that can help you as an implementation example:
STM32Cube_FW_F7_V1.16.0\Projects\STM32746G-Discovery\Applications\LwIP\LwIP_HTTP_Server_Netconn_RTOS
For more details about LwIP, please refer to this UM1713 : “Developing applications on STM32Cube with LwIP TCP/IP stack�?.
Imen
2021-01-29 12:11 AM
Hello @sunil and welcome to the STM32 Community 😊,
Have a look to the LwIP example under STM32CubeF7 MCU package, that can help you as an implementation example:
STM32Cube_FW_F7_V1.16.0\Projects\STM32746G-Discovery\Applications\LwIP\LwIP_HTTP_Server_Netconn_RTOS
For more details about LwIP, please refer to this UM1713 : “Developing applications on STM32Cube with LwIP TCP/IP stack�?.
Imen
2021-02-05 07:42 PM
Hi @Imen DAHMEN ,
Thanks for your support. I have tried LwIP_HTTP_Server_Netconn_RTOS from the example code and it works in NUCLEO-F746ZG. and also i searched example for SOCKET_API but it is not there for this NUCLEO-F746ZG board. I tried on own with help of STM example from some other board. The initialization was working fine but during entering IP address
it return the value -1
ret1 = read(conn, recv_buffer, buflen);
if(ret1 < 0) return;
and the full http-server-socket code is
void http_server_serve(int conn)
{
int buflen = 1500;
//int ret;
struct fs_file file;
unsigned char recv_buffer[1500];
/* Read in the request */
ret1 = read(conn, recv_buffer, buflen);
if(ret1 < 0) return;
/* Check if request to get ST.gif */
if (strncmp((char *)recv_buffer,"GET /STM32F7xx_files/ST.gif",27)==0)
{
fs_open(&file, "/STM32F7xx_files/ST.gif");
write(conn, (const unsigned char*)(file.data), (size_t)file.len);
fs_close(&file);
}
/* Check if request to get stm32.jpeg */
else if (strncmp((char *)recv_buffer,"GET /STM32F7xx_files/stm32.jpg",30)==0)
{
fs_open(&file, "/STM32F7xx_files/stm32.jpg");
write(conn, (const unsigned char*)(file.data), (size_t)file.len);
fs_close(&file);
}
/* Check if request to get ST logo.jpeg */
else if (strncmp((char *)recv_buffer,"GET /STM32F7xx_files/logo.jpg", 29) == 0)
{
fs_open(&file, "/STM32F7xx_files/logo.jpg");
write(conn, (const unsigned char*)(file.data), (size_t)file.len);
fs_close(&file);
}
else if(strncmp((char *)recv_buffer, "GET /STM32F7xxTASKS.html", 24) == 0)
{
/* Load dynamic page */
DynWebPage(conn);
}
else if((strncmp((char *)recv_buffer, "GET /STM32F7xx.html", 19) == 0)||(strncmp((char *)recv_buffer, "GET / ", 6) == 0))
{
/* Load STM32F7xxpage */
fs_open(&file, "/STM32F7xx.html");
write(conn, (const unsigned char*)(file.data), (size_t)file.len);
fs_close(&file);
}
else
{
/* Load 404 page */
fs_open(&file, "/404.html");
write(conn, (const unsigned char*)(file.data), (size_t)file.len);
fs_close(&file);
}
/* Close connection socket */
close(conn);
}
/**
* @brief http server thread
* @param arg: pointer on argument(not used here)
* @retval None
*/
static void http_server_socket_thread(void *arg)
{
int sock, newconn, size;
struct sockaddr_in address, remotehost;
int buflen = 1500;
struct fs_file file;
unsigned char recv_buffer[1500];
/* create a TCP socket */
if ((sock = socket(AF_INET, SOCK_STREAM, 0)) < 0)
{
return;
}
/* bind to port 80 at any interface */
address.sin_family = AF_INET;
address.sin_port = htons(80);
address.sin_addr.s_addr = INADDR_ANY;
if (bind(sock, (struct sockaddr *)&address, sizeof (address)) < 0)
{
return;
}
/* listen for incoming connections (TCP listen backlog = 5) */
listen(sock, 5);
size = sizeof(remotehost);
while (1)
{
newconn = accept(sock, (struct sockaddr *)&remotehost, (socklen_t *)&size);
http_server_serve(newconn);
}
}
and is there any STM example for websocket message transferring
I didn't find any STM example for LWIP for the STM32F407. If it there please provide the link
2021-02-05 11:36 PM
I found that problem in socket accept function
see the attach picture
it returns value newconn as -1 with listen(sock,5) and also listen(sock,8)
2021-02-05 11:36 PM