cancel
Showing results for 
Search instead for 
Did you mean: 

we want to use serial boot loader in stm32f765 ?

srikanth
Associate III

We are using stm32f765 serial boot loader to flash application code(.hex file) with USART1 (PA9,PA10). we connecting boot0 pin vcc (3.3v). But device memory is not detected and also device part is also not available for this what may be the resion .

1 REPLY 1

Didn't you ask the same question yesterday?

Are you using STM32 Cube Programmer application?

Can you see internal memory and ROM with a debugger?​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..