2010-02-07 12:59 PM
Virtual COM port in Win7 or Vista 32-bit
#stm32 #stm32 #stm32 #lmgtfy #stm32-virtual-com-port-vista-windows-72011-05-17 4:39 AM
Hello,
Thank you for your .inf file and the screenshots. I tried the inf file immediatly on my Vista, but the same Code 10 error is happening. Am i doing something wrong wirhin the code ? I'll try to debug the code and hopefully i find the problem. Thanks for now, b2011-05-17 4:39 AM
Hi bsmisl,
Here you go : new Driver ''stmcdc.zip'' which contains only one .inf file compliant with all Microsoft Windows Operating system so far including Windows 7 ( either x86 or x64 ). For full proof, I have attached the Screen shots that show that it is working properly with Windows 2000 Windows XP Windows Vista (x86 and x64) Windows 7 (x86 and x64) Enjoy it2011-05-17 4:39 AM
Hi ,
You can also
refer to the following article for an explanation of what error code 10 at Microsoft :
Explanation of error codes generated by Device Manager
http://support.microsoft.com/kb/310123
Follow the steps listed for Error Code 10 to see if that helps to resolve your issue or not.
Please post back to let us know if this information was helpful or not so that we may further assist you if need be.
Cheers,
STOne-32.
2011-05-17 4:39 AM
Hello,
About the Code 10 error, i found nothing usefull, my device is still not working under Vista or Win7. I think it might be something in the code. I have done some USB sniffing with the SnoopyPRO but i do not know if any thing is wrong. Has any one have the sniffers log, from the Vista or Win7 ? I hope i find something to fix this. Thanks, b2011-05-17 4:39 AM
Good day,
I got it to work on all OS. The problems were in the buffer sizes, that i fixed and it all works like a charm now. Well, thank you all for help, Greets, b2011-05-17 4:39 AM
Well done
2011-05-17 4:39 AM
2011-05-17 4:39 AM
I've the same issue. If I don't set buffer size to 64, I get error 10 in Windows. Is this normal? There's a way to use a greater buffer?
2011-05-17 4:39 AM
Dear all,
WHQL / Microsoft certified CDC (Serial driver) available on web
We have uploaded a new automatic install of new certified WHQL driver on Microsoft ( 2000 , XP, Vista and W7 : x86 and x64) : 1.3.1 for CDC driver
http://www.st.com/stonline/products/support/micro/files/VCP_Setup.zip
It is also available at Windows Update web Site as well. Cheers, STOne-32