User Activity

Hello.I have a custom board with STM32F750 MCU which has 64KB Internal Flash. Since the MCU's internal Flash is very limited i added external flash to board. I developed 2 different projects for Internal and External Flash. Internal Project starts wi...
Hello.I try develop TouchGFX+FreeRTOS based project for my custom board.I have a text area problem. I attached photo. Also project attached.It is not stable. It looks like always updating.Also when i touch the buttons other text areas looks same just...
Hello everyone.I have my custom board.STM32F750Z8 CPU with MT25QL128ABA External Flash.I don't have external RAM. My application code runs at External Flash. It is a simple code. I create just one screen at the TouchGFX and add two buttons. No other ...
Kudos from
Kudos given to