2020-12-10 8:25 AM
I use
I tried to assign systic to timer 14
I wanted to use timer8 for something else.
I enabled "HAL_REGISTER_CALLBACK" for timers.
When the system starts, during "HAL_Init()" timer14 is initialized as systic timer and immediately started with IRQ service. HAL_TIM_Base_Start_IT(&htim14);
But TIM14 shares IRQ with Timer 8 and timer 8 is not initialized yet.
So the IRQ handler is called, and it calls
void TIM8_TRG_COM_TIM14_IRQHandler(void)
{
/* USER CODE BEGIN TIM8_TRG_COM_TIM14_IRQn 0 */
/* USER CODE END TIM8_TRG_COM_TIM14_IRQn 0 */
HAL_TIM_IRQHandler(&htim8);
HAL_TIM_IRQHandler(&htim14);
/* USER CODE BEGIN TIM8_TRG_COM_TIM14_IRQn 1 */
/* USER CODE END TIM8_TRG_COM_TIM14_IRQn 1 */
}
But Timer 8 is not initialized yet.
In HAL_TIM_IRQHandler for timer 8, callback functions are called, which are not initialized. (=NULL) which causes a Null Pointer Exception.
What is the correct setting to avoid this? I see no way to move the timer initialisation before HAL Systick initialization.
I use a workaround like this:
void TIM8_TRG_COM_TIM14_IRQHandler(void)
{
/* USER CODE BEGIN TIM8_TRG_COM_TIM14_IRQn 0 */
if(htim8.State!=HAL_TIM_STATE_RESET)
HAL_TIM_IRQHandler(&htim8);
if(htim14.State!=HAL_TIM_STATE_RESET)
HAL_TIM_IRQHandler(&htim14);
return;
/* USER CODE END TIM8_TRG_COM_TIM14_IRQn 0 */
HAL_TIM_IRQHandler(&htim8);
HAL_TIM_IRQHandler(&htim14);
/* USER CODE BEGIN TIM8_TRG_COM_TIM14_IRQn 1 */
/* USER CODE END TIM8_TRG_COM_TIM14_IRQn 1 */
}
What do I miss out?
Thank you for your help
Johannes