2024-05-21 02:10 AM
Hi,
I'm a little lost, I would like to use the alternative6 (AF6) function on my stm32f405. I tried to do it via cube mx by configuring the pins but the generated code seems strange to me :
So for me I'd like to use SPI3 with PB3/4/5 so AF6 in datasheet. But if I configured that on cubemx I got this:
static void MX_SPI3_Init(void)
{
/* USER CODE BEGIN SPI3_Init 0 */
/* USER CODE END SPI3_Init 0 */
/* USER CODE BEGIN SPI3_Init 1 */
/* USER CODE END SPI3_Init 1 */
/* SPI3 parameter configuration*/
hspi3.Instance = SPI3;
hspi3.Init.Mode = SPI_MODE_MASTER;
hspi3.Init.Direction = SPI_DIRECTION_2LINES;
hspi3.Init.DataSize = SPI_DATASIZE_8BIT;
hspi3.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi3.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi3.Init.NSS = SPI_NSS_SOFT;
hspi3.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_2;
hspi3.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi3.Init.TIMode = SPI_TIMODE_DISABLE;
hspi3.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi3.Init.CRCPolynomial = 10;
if (HAL_SPI_Init(&hspi3) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SPI3_Init 2 */
/* USER CODE END SPI3_Init 2 */
}
And for GPIO init
static void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
/* USER CODE BEGIN MX_GPIO_Init_1 */
/* USER CODE END MX_GPIO_Init_1 */
/* GPIO Ports Clock Enable */
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
/*Configure GPIO pin Output Level */
HAL_GPIO_WritePin(GPIOC, LED_R_Pin|LED_G_Pin|LED_B_Pin, GPIO_PIN_SET);
/*Configure GPIO pins : LED_R_Pin LED_G_Pin LED_B_Pin */
GPIO_InitStruct.Pin = LED_R_Pin|LED_G_Pin|LED_B_Pin;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
/* USER CODE BEGIN MX_GPIO_Init_2 */
/* USER CODE END MX_GPIO_Init_2 */
}
So for me thuis function is strange why I don't see somewhere Alternate_function use ?
Solved! Go to Solution.
2024-05-21 02:12 AM - edited 2024-05-21 05:35 AM
Hello,
Check the stm32f4xx_hal_msp.c file.
All the AFs which are configured with CubeMx are located in the msp file.
2024-05-21 02:12 AM - edited 2024-05-21 05:35 AM
Hello,
Check the stm32f4xx_hal_msp.c file.
All the AFs which are configured with CubeMx are located in the msp file.
2024-05-21 05:33 AM
nice thanks everything is clear now